1. Overview
The document will guide you through checking how to perform homing using a sensor connecting to an IO Module for a Rotary Actuator V2 instead of using the motor’s endstop. For more details about the Rotary Actuator V2, please refer to our site.
2. Setup Requirements
Components
- MachineMotion V2
P/N: CE-CL-010-0004 - Non-Flush Inductive Proximity Sensor
P/N: CE-SN-004-0001 - IO Module V1 - P/N: CE-MD-001-0000
Or IO Module V2 - P/N: CE-MD-001-0000 v2- IO Module’s address - Please see IO Module Address Configuration Guide
Input pin number that the Non-Flush Inductive Proximity Sensor is connected to
- IO Module’s address - Please see IO Module Address Configuration Guide
- NEMA 34 Stepper Servo Motor
Large - 157mm - P/N: MO-SM-011-0000
Medium - 100mm - P/N: MO-SM-012-0000
Small - 68mm - P/N: MO-SM-013-0000 - Rotary Actuator V2 with Sensor Provision
P/N: MO-RM-002-0001__3
Components Setup
Sensor to IO Module V1

Figure 1. Sensor to IO Module V1 connection
Sensor Trigger and Sensor Placement
The home final position will be right before the trigger piece.

Figure 2. The sensor at home position
Note: the sensor will need to be close and able to read the entire length of the sensor trigger piece as shown in the sample image below

Figure 3. Recommended distance between sensor and trigger piece

Figure 4. Sensor needs to pass in full length alignment directly on top of the trigger piece
Python Script
Variables
Before running the Homing with IO Module python script, a few variables below will need to be changed to match with your existing system connection and hardware.
To determine IO address, please consult the IO Module Address Configuration guide.
rotary_axis = 1 #can change depending on which drive port is used (drive 1, 2, 3 or 4)
speed_fast = 200 #deg/s, recommended max speed=300 deg/s
speed_slow = 10 #deg/s, recommended max speed = 10 deg/s for position accuracy
stop_accel = 400 #deg/s2, max 500deg/s2
IO_NetworkID = 4 #To be set depending on IO address
home_sensor_IOpin = 0 #read IO pin 0 (choose between 0,1,2,3)
motor_size=MOTOR_SIZE.LARGE #to change depending on existing motor (LARGE / MEDIUM / SMALL)
Motor Configuration
Make sure to match the motor configuration to your system with respect to the axis, actuator type, positive direction, current delivered to motor and motor size.
# config motor
# Note: make sure to add the correct positive direction (clockwise or counter_clockwise)
mm.configServo(rotary_axis, MECH_GAIN.indexer_v2_deg_turn, counter_clockwise, 10.0, motor_size)
For more details on MachineMotion Python API, please refer to our Github
3. Code Sequence Walkthrough
Sequence Flowchart

Full Python Script
import sys
sys.path.append("/var/lib/cloud9/vention-control/python-api")
import urllib.parse
from MachineMotion import *
mm = MachineMotionV2()
# When starting a program, one must remove the software stop before moving
print("--> Removing software stop")
mm.releaseEstop()
print("--> Resetting system")
mm.resetSystem()
# Detect all connected digital IO Modules
detectedIOModules = mm.detectIOModules()
home_position = 0 #deg
clockwise = DIRECTION.NORMAL #clockwise direction is positive
counter_clockwise = DIRECTION.NEGATIVE #counterclockwise direction is positive
max_rotation_distance = 360 #(deg) 1 full rotation
#The following variables can be changed based on your system set up
rotary_axis = 1 #can change depending on which drive port is used (drive 1, 2, 3 or 4)
speed_fast = 200 #deg/s, recommended max speed=300 deg/s
speed_slow = 10 #deg/s, recommended max speed = 10 deg/s for position accuracy
stop_accel = 400 #deg/s2, max 500deg/s2
IO_NetworkID = 4 #To be set depending on IO address
home_sensor_IOpin = 0 #read IO pin 0 (choose between 0,1,2,3)
motor_size=MOTOR_SIZE.LARGE #to change depending on existing motor (LARGE / MEDIUM / SMALL)
#defining sensor detected function (read pin and return pin value if sensor is triggered (triggered == 0))
def sensor_detected():
pin_value = mm.digitalRead(IO_NetworkID, home_sensor_IOpin)
print(f'Stage {stage_number}: pin {home_sensor_IOpin} on {IO_NetworkID} has value {pin_value}')
return pin_value == 0
# config motor
# Note: make sure to add the correct positive direction (clockwise or counter_clockwise)
mm.configServo(rotary_axis, MECH_GAIN.indexer_v2_deg_turn, counter_clockwise, 10.0, motor_size)
# Stage 1: Move fast until sensor is triggered (locate sensor position)
stage_number = 1
#detect conecting IO module(s)
if detectedIOModules is not None :
#WARNING: THIS WILL MAKE THE SERVO MOVES BETWEEN 0-360 deg until the sensor is detected, depending on the starting position
#set speed to find home then start move in the positive direction
mm.setSpeed(speed_fast)
mm.moveRelative(rotary_axis, max_rotation_distance)
#move until sensor is triggered
while True:
if sensor_detected():
mm.stopContinuousMove(rotary_axis, stop_accel)
break
# Stage 2: Move backward slow, ensuring the senser trigger piece is on the sensor
stage_number = 2
# setspeed - very slow then start move in the negative direction
mm.setSpeed(speed_slow)
print("low speed")
mm.moveRelative(rotary_axis, -max_rotation_distance)
print("reverse move")
# condition if trigger piece has stop pass sensor, continue move negative until the sensor is triggered
if not sensor_detected():
while True:
if sensor_detected():
break
# Stage 3: verified the trigger piece is on top of the sensor
# continue in the negative direction and stop at position right before trigger piece (accurate position), set current position to 0
stage_number = 3
while True:
if not sensor_detected():
mm.stopContinuousMove(rotary_axis, stop_accel)
print("home_ready, position set to 0")
mm.setPosition(rotary_axis,home_position)
break
time.sleep(0.1)
# Vention Homing with IO solution for Rotary Actuator V2
Potential Features
It is possible to add more future to the Homing with IO Module Python script such as:
- Run script automatically on startup
- Run script when a button is pressed
- Read motor position value, motor return to near 0 position and then homing sequence starts
Comments
0 comments
Please sign in to leave a comment.